hi Miss/Sir:
I have two questions about TCL Script for auto-programming.Could u help? thanks in advanced.
1) How to handle the exception in following tcl code ,when running tcl in codewarrior.
When error occurs, the execution will stop. How to go end,if error occurs
fl::disconnect
fl::target -lc "LC
for Simple Flash"
fl::target -b 0xf400
0xc00
fl::target -v off -l off
cmdwin::fl::device -d
"MC56F82748_P_FLASH" -o "32kx16x1" -a 0x0 0x7fff
cmdwin::fl::image -f “c:\\FW.s" -t "Auto Detect" -re on -r 0x0 0x7fff -oe off
cmdwin::fl::erase all
cmdwin::fl::write
cmdwin::fl::device -d "MC56F82748_X_FLASH" -o "32kx16x1" -a 0x4000 0xbfff
cmdwin::fl::image -f “c:\\FW.s" -t "Auto Detect" -re on -r 0x4000 0xbfff -oe off
cmdwin::fl::erase all
cmdwin::fl::write
fl::disconnect
#End:
log s c:\\resultlog.txt
quitIDE
2) Could I replace “f1:erase image” with “f1::erase all?
“f1::erase all” takes less time than "f1::erase image".
已解决! 转到解答。
Hello Hillz
In Classic CodeWarrior for DSC, the debugger shell supports using “config” command to control whether the script will continue after an error. The command is:
config onScriptError abort | continue
However I tested on Eclipse CodeWarrior, this command is not supported and I cannot find the equivalent command. All the commands supported are listed in Chapter 4 <Debugger Shell> in CodeWarrior Development Studio Common Features Guide:
http://cache.nxp.com/files/soft_dev_tools/doc/user_guide/CWCFUG.pdf
For the second question, there is no any problem to replace “f1:erase image” with “f1::erase all”.
Best Regards
Fiona Kuang
Technical Information & Commercial Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Hillz
In Classic CodeWarrior for DSC, the debugger shell supports using “config” command to control whether the script will continue after an error. The command is:
config onScriptError abort | continue
However I tested on Eclipse CodeWarrior, this command is not supported and I cannot find the equivalent command. All the commands supported are listed in Chapter 4 <Debugger Shell> in CodeWarrior Development Studio Common Features Guide:
http://cache.nxp.com/files/soft_dev_tools/doc/user_guide/CWCFUG.pdf
For the second question, there is no any problem to replace “f1:erase image” with “f1::erase all”.
Best Regards
Fiona Kuang
Technical Information & Commercial Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------