Hello:
I use CW10.6, and download code to TRK-KEA128 by debug configurations (by OpenSDA), and do on-line testing for a while.
Now I need to keep the firmware when pull-out from debug, so I won't download every time when I want do a test. What options should I select in CW?
Thanks,
Hello Kuan,
Do you want run the project without CW IDE.
If yes,
You needn't do nothing else , after you download your project into your
board, now ,you can re-insert the USB , it can work well , you can test one simple
project , for example hello world or LED demo .
If i misunderstand your meaning, please tell me .
Hope it helps!
Have a great day,
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
hello,
I have my easy project to play a blink LED on TRK-KEA128
when I use debug it works well, and press reset switch
then start at "__init_registers();" and resume also continue blink well.
Somehow, when I disconnect the debug (still keeping blink),
and then try press reset switch, then the led is never blink again.
that's why I say the code wasn't mount in the memory, and if any debug setting is necessary but I missed, please tell me, thank you