I am trying to compile and flash the NXP sensor funsion rev 5 and trying to following the instructions using a K64f freedom board with codewarrior 10.7 (latest one just downloaded for windows 7. I am using the opensda and receiving the following error when I do a run configuration:
Error launching FRDM-k64F_MQLX_FLASH_OpenSDA ARM GDI Protocol Adapter. Cannot connect . The Debugger can not connect to the P&E Device.
I have no idea what I am doing as this is my first experience with MBED - coming from a Arduino background. So keep it simple
THanks
Mike
Hi,
I suggest you check the problem with below steps.
1. create a new work space.
2. create a new project in this workspace, test if the connection can work.
3. if it fails connection in step2, please update the FRDM board driver with referring this article
https://community.nxp.com/docs/DOC-105199
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Jennie
Your post helped alot. It appears that if I use CodeWarrior I have to use segger and if I want the board to act like a drive like for the sensor toolbox v5 I need to set it up like mned and just let it load the bin. Broke the code with your help.
Thanks
Mike
Hi Mike,
Good to know. You are welcome!
Best Regards,
Jennie