ColdFire Bareboard "Vx Evaluation Boards" sample project not longer available in CodeWarrior for MCU 10.5

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ColdFire Bareboard "Vx Evaluation Boards" sample project not longer available in CodeWarrior for MCU 10.5

ソリューションへジャンプ
835件の閲覧回数
desroc01
Contributor II


Hello,

 

With Code Warrior for MCU 10.1, it was possible to select the category "ColdFire Vx Evaluation Boards" devices type in the "Bareboard" (New Project Wizard).

 

Now, I installed Code Warrior for MCU 10.5 and the category "ColdFire Vx Evaluation Boards" devices is NOT there anymore. That is a pity because "ColdFire Vx Evaluation Boards" contains all code for the EVB and DEMO dev kit.

 

Is there a way to import the "ColdFire Vx Evaluation Boards" demo project in Code Warrior for MCU 10.5 ?

Where can I download these demo projects ? (add on?)

 

Thanks for your time,

ラベル(1)
0 件の賞賛
返信
1 解決策
667件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello desroc01

The stationery for “ColdFire Vx Evaluation Boards" is removed from CodeWarrior v10.3.

You can keep both CodeWarrior version v10.1 and v10.5 on your PC, and after creating the project in CW10.1 with "ColdFire Vx Evaluation Boards" stationery, import it into CodeWarrior v10.5.

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
668件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello desroc01

The stationery for “ColdFire Vx Evaluation Boards" is removed from CodeWarrior v10.3.

You can keep both CodeWarrior version v10.1 and v10.5 on your PC, and after creating the project in CW10.1 with "ColdFire Vx Evaluation Boards" stationery, import it into CodeWarrior v10.5.

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
667件の閲覧回数
ssinfod
Contributor IV

Any idea why it was removed ?

Would it be possible for nxp/freescale to create an "extension pack" which contains ColdFire Vx Evaluation Boards" demo projects and others samples (for other MCU).

In my case, it took me a lot of time to find the demo project of the M52233DEMO board.

Thanks,

0 件の賞賛
返信