CW4.6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决
1,673 次查看
daistar
Contributor I
how long will i get a copy of CW4.6 evaluation copy????
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
636 次查看
CrasyCat
Specialist III
Hello
 
Did you order a CD and are you waiting for the CD or are you waiting for a license?
 
You should be able to download the software from the web.
Go to the CodeWarrior for HC12 product page
And download the special edition.
 
Software comes with a special edition allowing you to process up to 32K of C source code.
 
CrasyCat

在原帖中查看解决方案

0 项奖励
回复
2 回复数
637 次查看
CrasyCat
Specialist III
Hello
 
Did you order a CD and are you waiting for the CD or are you waiting for a license?
 
You should be able to download the software from the web.
Go to the CodeWarrior for HC12 product page
And download the special edition.
 
Software comes with a special edition allowing you to process up to 32K of C source code.
 
CrasyCat
0 项奖励
回复
637 次查看
J2MEJediMaster
Specialist I
I don't really understand what you want from such a brief question. I'll try to answer anyway. You can go get the CodeWarrior HCSX(12) page here and follow the Special Edition link to download an evaluation copy of CW 4.6. (I'm assuming you're wanting to use HCS12(X), based on the version number.) Don't forget to downoad the license file, which is typically good for 30 days. Study the charts on that page to understand what the limitations of the Special Edition are before downloading.

---Tom



Message Edited by J2MEJediMaster on 2007-05-29 07:45 AM