CW10.7 Some update sites could not be found - DSC 56F8037

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW10.7 Some update sites could not be found - DSC 56F8037

722 Views
j___
Contributor IV

Using CW 10.7 for a DSC project. I found a pretty annoying compiler issue (bug). So, I wanted to see if there is an updated compiler for the 56F8037. Using Help-Check for Updates, I got the following messages:

Some sites could not be found.  See the error log for more detail.
No repository found at http://www.pemicro.com.
No repository found at jar:file:C:%5CUsers%5CLAB%5CDownloads%5CFreescale%5CCW10.7%5CCW%20for%20MCU%2010.7%5Ccom.freescale.mcu10_7.hcs08_rs08.updatesite.zip!/.
No repository found at jar:file:C:%5CUsers%5CLAB%5CDownloads%5CFreescale%5CCW10.7%5CCW%20for%20MCU%2010.7%5Ccom.freescale.mcu10_7.s12z.updatesite.zip!/.
Unable to read repository at http://nxp.com/lgfiles/updates/Eclipse/MCU10_7/updatesite/content.xml.
sun.security.validator.ValidatorException: PKIX path building failed: sun.security.provider.certpath.SunCertPathBuilderException: unable to find valid certification path to requested target
No repository found at jar:file:C:%5CUsers%5CLAB%5CDownloads%5CFreescale%5CCW10.7%5CCW%20for%20MCU%2010.7%5Ccom.freescale.mcu10_7.kinetis.updatesite.zip!/.
No repository found at jar:file:C:%5CUsers%5CLAB%5CDownloads%5CFreescale%5CCW10.7%5CCW%20for%20MCU%2010.7%5Ccom.freescale.mcu10_7.e200.updatesite.zip!/.
No repository found at jar:file:C:%5CUsers%5CLAB%5CDownloads%5CFreescale%5CCW10.7%5CCW%20for%20MCU%2010.7%5Ccom.freescale.mcu10_7.dsc.updatesite.zip!/.
No repository found at jar:file:C:%5CUsers%5CLAB%5CDownloads%5CFreescale%5CCW10.7%5CCW%20for%20MCU%2010.7%5Ccom.freescale.mcu10_7.coldfire.updatesite.zip!/.

When will these repositories be back up and working?

How can I manually check what the revision history of all DSC compilers that are compatible with CW10.7?

Once I (manually via webpage?) know the compiler history and changes log, how can I manually download the updated compiler that I want?

0 Kudos
Reply
1 Reply

536 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Please try offline updates. You can download them with following attached video.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply