CW? - S08GT60 MC13192 - ADC conversion sent over SMAC Where do I start??

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW? - S08GT60 MC13192 - ADC conversion sent over SMAC Where do I start??

Jump to solution
1,967 Views
ehestigoni
Contributor III
Hi Guys,

I have just started to use codewarrior and need some advice...
I have 2 boards with MC9S08GT60 mcu and  MC13192 transc on. I will be receiving my USBMULTILINK in few days and I wanna get started using the simulation first.

In the end, I will need to write a code to collect samples from the AD using the mcu MC9S08GT60 on one of the boards and transmit to the other.

So, I was wondering if there is a template to start working on.
I've downloaded the BeeKit, and I created some projects to export to CodeWarrior. But I didn't really get the idea yet... Is it the best way to go? Or should I start doing something with the AD first and then try to add the SMAC stuff?

Cheers,

Ed.

--
Alban Edit: FSL Part Number must figure in Message Subject line.





Message Edited by Alban on 2007-08-01 11:38 AM
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
908 Views
ehestigoni
Contributor III
Sorry my mistake.
 
CW is 6.0, I've just downloaded it.
I will read more about it before come with questions.
 
Cheers,
 
Ed.
 
 

View solution in original post

0 Kudos
Reply
2 Replies
908 Views
Alban
Senior Contributor II
Hello Ed,

May you please start by indicating the CodeWarrior version + the device you are using in the subject line ?
Have a descriptive subject allow person willing to contribute to spot the type of subjects they can attend.

You can have a look at the 8-Bit MCU board as a lot of info on the SMAC and ZigBee is available there.
It will also give you links to examples and sample code.

The search engine at the bottom of Forum pages will help you to find pertinent posts.

Cheers,
Alban.


909 Views
ehestigoni
Contributor III
Sorry my mistake.
 
CW is 6.0, I've just downloaded it.
I will read more about it before come with questions.
 
Cheers,
 
Ed.
 
 
0 Kudos
Reply