Example MPC5644A External SRAM - CodeWarrior for MCUs v10.5

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example MPC5644A External SRAM - CodeWarrior for MCUs v10.5

Example MPC5644A External SRAM - CodeWarrior for MCUs v10.5

The example demonstrates project adjustments required in order to run and debug the code running from external SRAM rather then from internal memory.

This example performs basic initialization and runtime EBI interface configuration (FLASH Build target) so the external SRAM memory becomes available while executing the code (without debugger).

The debugger launching TCL script (\Project_Settings\Debugger\MPC5644A_VLE.tcl, init_ebi()) has been adjusted to load program into external SRAM (EXT_SRAM)

 

Test HW:  MPC5644A + XPC564A minimodule + XPC56XX mother board

Maskset:  OM14X

Target :  External SRAM, Internal FLASH

Fsys:     16MHz IRC


Debugger: PeMicro USB-ML-PPCNEXUS

IDE/Compiler: CodeWarrior for MCUs v10.5

EVB connection:
  Default EVB jumper setup

Attachments
No ratings
Version history
Last update:
‎09-30-2019 07:43 AM
Updated by: