Example MPC5644A External SRAM - CodeWarrior for MCUs v10.5

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Example MPC5644A External SRAM - CodeWarrior for MCUs v10.5

Example MPC5644A External SRAM - CodeWarrior for MCUs v10.5

The example demonstrates project adjustments required in order to run and debug the code running from external SRAM rather then from internal memory.

This example performs basic initialization and runtime EBI interface configuration (FLASH Build target) so the external SRAM memory becomes available while executing the code (without debugger).

The debugger launching TCL script (\Project_Settings\Debugger\MPC5644A_VLE.tcl, init_ebi()) has been adjusted to load program into external SRAM (EXT_SRAM)

 

Test HW:  MPC5644A + XPC564A minimodule + XPC56XX mother board

Maskset:  OM14X

Target :  External SRAM, Internal FLASH

Fsys:     16MHz IRC


Debugger: PeMicro USB-ML-PPCNEXUS

IDE/Compiler: CodeWarrior for MCUs v10.5

EVB connection:
  Default EVB jumper setup

附件
无评分
版本历史
最后更新:
‎09-30-2019 07:43 AM
更新人: