Where can I download CodeWarrior HC12 V5.90 build 5294?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Where can I download CodeWarrior HC12 V5.90 build 5294?

777 次查看
dementeddigital
Contributor II

The Freescale download link no longer works.

Here is the old link: http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-HCS12X&tid=CWH

0 项奖励
1 回复

572 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Dan,

Please download it at here :

CodeWarrior® Dev Tools for HCS12(X) MCUs|NXP  

pastedImage_3.png

If you want download CW HC12 v5.1  , please select "Prerious" , then you can find it :

pastedImage_2.png

The two version all are the CW IDE you mentioned .

pastedImage_4.png

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励