I can not erase the nor flash on the twr8309 board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I can not erase the nor flash on the twr8309 board

640件の閲覧回数
jinxiaofei
Contributor I

My codewarrior version is 10.4,and when I burning my own boot to the twr 8309 board.There is an error:

Error:  Connect Failed.

Could not connect to the probe (or other debug link)

[CCS last error: CC config string is invalid ](CCSProtocolPlugin)

Error: Connect Failed.

and I open the jtag diagnostics.It print the message "Error measuing IR length"

My windows's language is English.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

464件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello jin xiaofei,

Probably you destroyed RCW on the target board, please use the feature "CodeWarrior JTAG configuration file to override RCW", please refer to the section "Setting up a remote system to use a JTAG configuration file" in C:\Freescale\CW_PA_v10.5.0\PA\Help\PDF\Targeting_PA_Processors.pdf.

In addition, if you use the old product USB TAP, please change the connection type as "USB TAP".

If this problem remains, you need to consider about the hardware problem.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

464件の閲覧回数
addiyi
NXP Employee
NXP Employee

This error happens only after you program your own boot-loader? Before that you were able to connect to the board?

Adrian

0 件の賞賛
返信