I can not erase the nor flash on the twr8309 board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I can not erase the nor flash on the twr8309 board

935 Views
jinxiaofei
Contributor I

My codewarrior version is 10.4,and when I burning my own boot to the twr 8309 board.There is an error:

Error:  Connect Failed.

Could not connect to the probe (or other debug link)

[CCS last error: CC config string is invalid ](CCSProtocolPlugin)

Error: Connect Failed.

and I open the jtag diagnostics.It print the message "Error measuing IR length"

My windows's language is English.

Labels (1)
0 Kudos
Reply
2 Replies

759 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello jin xiaofei,

Probably you destroyed RCW on the target board, please use the feature "CodeWarrior JTAG configuration file to override RCW", please refer to the section "Setting up a remote system to use a JTAG configuration file" in C:\Freescale\CW_PA_v10.5.0\PA\Help\PDF\Targeting_PA_Processors.pdf.

In addition, if you use the old product USB TAP, please change the connection type as "USB TAP".

If this problem remains, you need to consider about the hardware problem.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

759 Views
addiyi
NXP Employee
NXP Employee

This error happens only after you program your own boot-loader? Before that you were able to connect to the board?

Adrian

0 Kudos
Reply