Will there ever be a version that runs on WIndows 64-bit?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Will there ever be a version that runs on WIndows 64-bit?

880 Views
LesleyF
Contributor I

Is there ever going to be support for Windows 7 64-bit?   It is becoming a problem because our IT department is stopping support for XP.  Any news on this? 

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

405 Views
trytohelp
NXP Employee
NXP Employee

Hi,

 

CodeWarrior for DSC V8.3 was designed for  XP/Vista 32 bit OS.

We don't have a version supporting Windows 7.

The next version is planned for end 2011.

DSC architecture will be integrated in CodeWarrior for MCU in the MCU10.2 release.

This version will support:

      Microsoft® Windows XP 32/64-bit (Business)

      Microsoft® Windows Vista 32/64-bit (Business and Home Premium)

      Microsoft® Windows 7 32/64-bit (Professional and Home Premium)

      Linux Red Hat Enterprise Edition 5.2 32-bit

 

I know some customers have already installed DSC tool on windows 7 but some of them (5% probably) were not able to run CodeWarrior under windows 7.

================================

- Run Windows 7 in Windows XP SP3 mode. Forward the USB ports to the XP VM.

 

Disable Desktop Composition:

      - Right click on ide.exe and select "Properties"

      - Click on the "Compatibility" tab

      - In the "Settings" area select "Disable Desktop Composition"

================================

 

I got a feedback from a customer ...

 

******************************

Now it runs relatively well, once I pass the initial opening and compiling phases of the project..

So afterwards, IDE seems to be able to communicate with the USB-TAP well enough, that I see no apparent problems running the “time-critical” project we have on the target board. (Like V22bis modem, etc.)..

 

The sections where CW8.3 seem to have problems with Windows 7 is when opening and closing the projects/files.. It is considerably slow.. But eventually it works.. As I said, this is better than not having CW at all..

 

This is what I was able to find out by trial and error, in order to get the CW8.3 running on Windows 7;

-          Right click IDE.exe in the \bin folder.

-          Select    “Properties”

-          Select    “Compatibility”

-          Select    “Change settings for all users”

-          Select    “Run this program in compatibility mode for”

-          Select    “Windows Vista” from pull down menu

-          Select    “Disable visual themes” & “Disable desktop composition” &” Disable display scaling on high DPI settings”.

-          Do NOT select  “Run in 256 colors” & “Run in 640x480 screen resolution”.

Hit OK 

 

 

******************************

 

I think you could run the build tool chain without problem under Windows 7.

the main issue is with USBtap ...

 

The quick solution should be to keep a PC on windows XP with the USBTap and to configure your Windows 7 CCS in remote.

By this way your Windows 7 could use the USBtap installed on XP.

 

Hope this will help you.

 

Regards

Pascal

0 Kudos
Reply