Problem on reprogram MC56F8006 if the unused I/O pins are initialized

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem on reprogram MC56F8006 if the unused I/O pins are initialized

ソリューションへジャンプ
1,905件の閲覧回数
Janio
Contributor I

Hello!

 

I was working with my project based on MC56F8006, when I tried to initialize unused I/O pins by the bean inspector. After initialize the unused pins as output with internal Pullup resistor, I programmed once and when I tried to run, the CCS returned me a connectivity error. I tried one more time to program and the CCS returned the following error message: "the device is not powered up", but it really was, and the program, loaded once, was running correctly.

 

My MC56F8006 is working, but I can't load the program anymore.. Or since I've initialized the unused pins as output with pullup resistor.

 

I've made this test with 2 prototype boards (handmade), loading the program with a parallel JTAG connection and the USB-TAP... The same error has occurred.. I hope find a way to load my FWs again.. Somebody help me please!

 

Regards,

 

Janio

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,020件の閲覧回数
Janio
Contributor I
Haha.. I know what was wrong.. I've configured the JTAG pins as Output.. (stupid boy).. To reprogram, before to run the FW, hold the reset button of the board to make the DSC enter on program mode (I don't know if it is the correct term), press the run button from CW, wait the conection starts and pull off the reset button to let CW load the FW. You must be "foxy" to pull off the button in the correct time, but it works! Regards, Janio

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,021件の閲覧回数
Janio
Contributor I
Haha.. I know what was wrong.. I've configured the JTAG pins as Output.. (stupid boy).. To reprogram, before to run the FW, hold the reset button of the board to make the DSC enter on program mode (I don't know if it is the correct term), press the run button from CW, wait the conection starts and pull off the reset button to let CW load the FW. You must be "foxy" to pull off the button in the correct time, but it works! Regards, Janio
0 件の賞賛
返信
1,020件の閲覧回数
believe
Contributor I

hi, are you Chinese? I am doing sensorless BLDC with MC56F8006,can we communication with 8006?

My mobile phone is :+86 13705541506,my QQ is 356119619,can we study with each other?

0 件の賞賛
返信