CWH-CTP-BASE-HE simulator can't connect P2020 Question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CWH-CTP-BASE-HE simulator can't connect P2020 Question

5,178 Views
wangrui_202077
Contributor I

Hi:

     I use the "CWH-CTP-BASE-HE" simulator to debug P2020 rgb board, and Download the codewarrior 10.5.1 (Windows)version for it, My PC use the Win7,  But Now I can't connect the simulator.  codewarrior connection error is : "ccsprotocolplugin: Could not connect to the probe (or other debug link) [CCS last error: cc not present." Did I lack of some patches? or any other Incorrect usage?

Hope Your reply!

0 Kudos
Reply
12 Replies

5,020 Views
wangrui_202077
Contributor I

Hello YiPing:

      I use codewarrior10.5.1 on win7, and create a P2020 project, use the following steps; others use default settings.
      Create a codewarrior Bareboard Project
      Next
      choose QorIQ_P2 P2020
      Next

      But when I build it, it stopped halfway with the following warnings. what's the reason?

build_console.PNG

warning.PNG

project.PNG

Thanks,

Rui 

0 Kudos
Reply

5,020 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Rui,

The file hello_world-core00.elf has already been generated, you could ignore this warning.

Thanks,

Yiping

0 Kudos
Reply

5,020 Views
wangrui_202077
Contributor I

您好!

      我调试的处理器是P2020,使用的调试器是CodeWarrior TAP;IDE使用CodeWarrior 8.8,创建了一个P2020的工程,connection protocals选择是CodeWarrior USB TAP,然后点击Debug时提示“The JTAG chain does not contain any debuggable cores!”。抓取的log如下,请帮忙解答下原因,非常感谢!

现象.PNGlogs.PNG

Thanks,

Rui 

0 Kudos
Reply

5,020 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Rui,

You need to download and install Patch 8.8.6 to update CCS USB driver, it can be downloaded from CodeWarrior Dev Tools for Networked Apps | NXP , please click DOWNLOAD-> 8.8 CodeWarrior DS for Power Architecture, Professional Edition(Windows Hosted) WIN Evaluation/Updates. 

If your problem remains, would you capture the whole CCS console log to me to do more investigation?

Thanks,

Yiping

0 Kudos
Reply

5,020 Views
wangrui_202077
Contributor I

您好啊!

我是用“64位Win7操作系统”、“Codewarrior REV G CWH-CTP-BASE-HE仿真器(支持USB和网络调试)”调试P2020开发板,

安装了如下软件:

CW_Power_Architecture_V8[1].8_Build_80229.exe

CW_PA_8_8_3_Build_90619.exe

CW_PA_V88_SP1_P1021-P1022.exe

CW PA v8.8.6 Windows – Patch.exe

CW_PA_V88_SP1_P2020-8572-8315-8569_Build_090819.exe

安装过程报错如下:

1.PNG

2.PNG

4.PNG

已经安装了您说的那个补丁,依然连不上仿真器,是不是codewarrior8.8 不能在64位win7操作系统上安装呀?调试出现如下错误:

cw8.8工程报错1.PNG

另外卸载掉codewarrior8.8,安装codewarrior10.5.1(CodeWarrior Development Studio for Power Architecture v10.5.1 - Windows .exe)也不能正常工作,报错也是这个cc not present,请问是缺少啥驱动或者补丁包啊?,

cw10.5.1-2.PNG

像我这样使用Codewarrior REV G CWH-CTP-BASE-HE仿真器(支持USB和网络调试)和64位win7操作系统应该使用哪个版本的codewarrior和哪些补丁包,才能正常调试P2020呢?请帮忙解答下,谢啦!

0 Kudos
Reply

5,020 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Rui Wang,

Please note, when installing CodeWarrior software, please plug off CodeWarrior TAP from your PC.

You could use CodeWarrior 10.5.1, please specify Connection type as "CodeWarrior TAP(over USB)" rather than "USB TAP" when creating a bareboard project.

In addition, please check whether CodeWarrior license is valid from Help->Freescale Licenses.

Thanks,

Yiping

0 Kudos
Reply

5,020 Views
wangrui_202077
Contributor I

HiYiping

       我的仿真器串口通过仿真器带的rj25转出来的与PC连接,串口也没有什么打印,波特率根据手册配置的115200,8,none,1,我的电脑串口连接板卡打印是正常的,串口本身没问题,这个信息有参考意义吗?新的仿真器是否需要烧什么配置呢?

0 Kudos
Reply

5,019 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please plug-in CodeWarrior TAP to your PC, wait for a moment, please check whether you could get similar information as the attachment in the device manager.

0 Kudos
Reply

5,020 Views
982576385
Contributor I

Hi Yiping Wang:

   I am using the same CW TAP and could not connect it too. The calss of emulator and the environment of mine are the same as @Rui Wang:cwh-tcp-base-he, win7 64bit ,CW 10.5.1 .And i did every thing he had mentioned. I can see the CW TAP in my device manager as you padded.   And i still can not connect it.

   What infomation in my ccs is the picture below,it is different from the CW 10.5 document"CodeWarrior TAP Probe User Guide" at page 46:pastedImage_1.jpg

  The result of configcc and show command as bellow,as the same with "protocol log" of CW IDE:USB open failure :

pastedImage_2.jpg

   And then ,what could i do? whether the hardware has broken?

Hope your reply.

0 Kudos
Reply

5,020 Views
wangrui_202077
Contributor I

HiYiping

License查看结果见附件,截取部分如下:好多插件是win32开头的?在win64 PC机上使用会受影响吗?同时我也在拔掉仿真器的情况下重新卸载干净后安装了codewarrior10.5.1软件,

功能Key

功能 WIN32_PLUGINS_DBG_PPC 10.5,状态: 15 

功能 WIN32_PLUGINS_GCC_Adapters 10.5,状态: 15 

功能 Win32_CFP_PPC 10.5,状态: 15 

功能 Win32_PLUGINS_PPCCPU_COMM 10.5,状态: 15 

功能 Win32_PLUGINS_PPCCPU_HOST 10.5,状态: 15 

功能 Win32_PLUGINS_PPCCPU_PQ3 10.5,状态: 15 

功能 Win32_Plugins_PPC_EmLinux 10.5,状态: 15 

替代Key

(没有key)

 

另外想问,咱们新买的codewarrior tap仿真器需要load进去什么配置文件嘛?使用仍然报cc not present这个错误,新建的工程debug配置选择是CodeWarrior TAP(over USB这个类型,请帮忙分析下原因,非常感谢!

license细节:

细节信息:产品"CodeWarrior Development Studio For PA" 版本"10.5"
状态:"License还有15天过期"
License
模式:"class com.freescale.core.ide.license.flexlm.FlexlmActivate11"
联系电子邮件:licensing@freescale.com
注册URLhttp://www.freescale.com/cwregister/
购买URL: http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW_DSPA&tid=CWH/
FlexLM
评估期还有:5
GTL
服务器:gtlsrvr.metrowerks.com
GTL
端口:80 (8,080)
需要Host ID: true
License
文件路径:D:\Freescale\CW_PA_v10.5.1\PA\license.dat
flexlmFileLocator: null
flexlmFile: ${PA_TOOLS_HOME}/license.dat
License
文件URL: file:/D:/Freescale/CW_PA_v10.5.1/eclipse/../PA/license.dat
错误字段:
Optional feature group #1:
Optional feature undefined: WIN32_PLUGINS_PPC 10.5
Group status: Included
Optional feature group #2:
Optional feature undefined: WIN32_PLUGINS_COMP_PPC 10.5
Optional feature undefined: Win32_Plugins_Link_PPC 10.5
Optional feature undefined: Win32_Plugins_Common_eLinux 2.3
Optional feature undefined: Win32_SA_Plugins_Trace_EPPC 10.5
Optional feature undefined: Win32_SA_Plugins_Perf_EPPC 10.5
Optional feature undefined: Win32_SA_Perf_EPPC 10.5
Optional feature undefined: Win32_SA_Perf_EPPC_ADVANCED 10.5
Group status: Included
Optional feature group #3:
Optional feature undefined: DDR_Validation_QorIQ 4.0
Optional feature undefined: SERDES_Validation_QorIQ 4.0
Optional feature undefined: PE_PACKETTOOL 4.5
Group status: Included
功能Key
功能 WIN32_PLUGINS_DBG_PPC 10.5,状态: 15
功能 WIN32_PLUGINS_GCC_Adapters 10.5,状态: 15
功能 Win32_CFP_PPC 10.5,状态: 15
功能 Win32_PLUGINS_PPCCPU_COMM 10.5,状态: 15
功能 Win32_PLUGINS_PPCCPU_HOST 10.5,状态: 15
功能 Win32_PLUGINS_PPCCPU_PQ3 10.5,状态: 15
功能 Win32_Plugins_PPC_EmLinux 10.5,状态: 15
替代Key
(
没有key)
LM_PATH=null
许可文件内容(D:\Freescale\CW_PA_v10.5.1\PA\license.dat)
~#CodeWarrior Development Studio v10 for Power Architecture
Technology
#(Eclipse) EVAL - CodeWarrior for Power Architecture - Professional Edition
#(Windows hosted) Evaluation / Updates for Rui Wang Software Account
# License for ANY
INCREMENT Win32_CFP_PPC metrowks 10.5 19-aug-2020 uncounted \
43F8E000D99F VENDOR_STRING="CodeWarrior for Power Architecture \
- Professional Edition (Windows hosted) Evaluation / Updates" \
HOSTID=ANY ISSUER="Freescale Semiconductor" ISSUED=20-jul-2020 \
NOTICE=NONE ck=129 SN="FSL - 31341727" TS_OK
# License for ANY
INCREMENT Win32_PLUGINS_COMMON_ELINUX metrowks 10.5 19-aug-2020 \
uncounted 2B08F4AE6471 VENDOR_STRING="CodeWarrior for Power \
Architecture - Professional Edition (Windows hosted) \
Evaluation / Updates" HOSTID=ANY ISSUER="Freescale \
Semiconductor" ISSUED=20-jul-2020 NOTICE=NONE ck=109 SN="FSL - \
31341727" TS_OK
# License for ANY
INCREMENT Win32_PLUGINS_COMP_PPC metrowks 10.5 19-aug-2020 uncounted \
F422A9C74775 VENDOR_STRING="CodeWarrior for Power Architecture \
- Professional Edition (Windows hosted) Evaluation / Updates" \
HOSTID=ANY ISSUER="Freescale Semiconductor" ISSUED=20-jul-2020 \
NOTICE=NONE ck=108 SN="FSL - 31341727" TS_OK
# License for ANY
INCREMENT Win32_PLUGINS_DBG_PPC metrowks 10.5 19-aug-2020 uncounted \
BA0B0E40E4DC VENDOR_STRING="CodeWarrior for Power Architecture \
- Professional Edition (Windows hosted) Evaluation / Updates" \
HOSTID=ANY ISSUER="Freescale Semiconductor" ISSUED=20-jul-2020 \
NOTICE=NONE ck=118 SN="FSL - 31341727" TS_OK
# License for ANY
INCREMENT Win32_PLUGINS_Link_PPC metrowks 10.5 19-aug-2020 uncounted \
65A7CFAF7328 VENDOR_STRING="CodeWarrior for Power Architecture \
- Professional Edition (Windows hosted) Evaluation / Updates" \
HOSTID=ANY ISSUER="Freescale Semiconductor" ISSUED=20-jul-2020 \
NOTICE=NONE ck=159 SN="FSL - 31341727" TS_OK
# License for ANY
INCREMENT Win32_Plugins_PPC_LNX metrowks 10.5 19-aug-2020 uncounted \
72B4FD4156EC VENDOR_STRING="CodeWarrior for Power Architecture \
- Professional Edition (Windows hosted) Evaluation / Updates" \
HOSTID=ANY ISSUER="Freescale Semiconductor" ISSUED=20-jul-2020 \
NOTICE=NONE ck=132 SN="FSL - 31341727" TS_OK
# License for ANY
INCREMENT Win32_PLUGINS_PPC metrowks 10.5 19-aug-2020 uncounted \
10BBC689DE31 VENDOR_STRING="CodeWarrior for Power Architecture \
- Professional Edition (Windows hosted) Evaluation / Updates" \
HOSTID=ANY ISSUER="Freescale Semiconductor" ISSUED=20-jul-2020 \
NOTICE=NONE ck=102 SN="FSL - 31341727" TS_OK
# License for ANY
INCREMENT Win32_Plugins_PPC_KDBG metrowks 10.5 19-aug-2020 uncounted \
3AB0A2653A3B VENDOR_STRING="CodeWarrior for Power Architecture \
- Professional Edition (Windows hosted) Evaluation / Updates" \
HOSTID=ANY ISSUER="Freescale Semiconductor" ISSUED=20-jul-2020 \
NOTICE=NONE ck=91 SN="FSL - 31341727" TS_OK
# License for ANY
INCREMENT Win32_PLUGINS_PPCCPU_COMM metrowks 10.5 19-aug-2020 \
uncounted E9DDB6BEBAAB VENDOR_STRING="CodeWarrior for Power \
Architecture - Professional Edition (Windows hosted) \
Evaluation / Updates" HOSTID=ANY ISSUER="Freescale \
Semiconductor" ISSUED=20-jul-2020 NOTICE=NONE ck=184 SN="FSL - \
31341727" TS_OK
# License for ANY
INCREMENT Win32_PLUGINS_PPCCPU_HOST metrowks 10.5 19-aug-2020 \
uncounted 2BFD4D48961E VENDOR_STRING="CodeWarrior for Power \
Architecture - Professional Edition (Windows hosted) \
Evaluation / Updates" HOSTID=ANY ISSUER="Freescale \
Semiconductor" ISSUED=20-jul-2020 NOTICE=NONE ck=131 SN="FSL - \
31341727" TS_OK
# License for ANY
INCREMENT Win32_PLUGINS_PPCCPU_PQ3 metrowks 10.5 19-aug-2020 \
uncounted F2061CDCD7F2 VENDOR_STRING="CodeWarrior for Power \
Architecture - Professional Edition (Windows hosted) \
Evaluation / Updates" HOSTID=ANY ISSUER="Freescale \
Semiconductor" ISSUED=20-jul-2020 NOTICE=NONE ck=105 SN="FSL - \
31341727" TS_OK
# License for ANY
INCREMENT Win32_SA_Plugins_Perf_EPPC metrowks 10.5 19-aug-2020 \
uncounted 589BC371D051 VENDOR_STRING="CodeWarrior for Power \
Architecture - Professional Edition (Windows hosted) \
Evaluation / Updates" HOSTID=ANY ISSUER="Freescale \
Semiconductor" ISSUED=20-jul-2020 NOTICE=NONE ck=38 SN="FSL - \
31341727" TS_OK
# License for ANY
INCREMENT Win32_SA_Plugins_Trace_EPPC metrowks 10.5 19-aug-2020 \
uncounted 0D1AE715BDD6 VENDOR_STRING="CodeWarrior for Power \
Architecture - Professional Edition (Windows hosted) \
Evaluation / Updates" HOSTID=ANY ISSUER="Freescale \
Semiconductor" ISSUED=20-jul-2020 NOTICE=NONE ck=182 SN="FSL - \
31341727" TS_OK
# License for ANY
INCREMENT Win32_SA_Plugins_Trace_Linux metrowks 10.5 19-aug-2020 \
uncounted 9F18B399CFF1 VENDOR_STRING="CodeWarrior for Power \
Architecture - Professional Edition (Windows hosted) \
Evaluation / Updates" HOSTID=ANY ISSUER="Freescale \
Semiconductor" ISSUED=20-jul-2020 NOTICE=NONE ck=163 SN="FSL - \
31341727" TS_OK
# License for ANY
INCREMENT Win32_SA_Perf_EPPC metrowks 10.5 19-aug-2020 uncounted \
6A0F6495D3C8 VENDOR_STRING="CodeWarrior for Power Architecture \
- Professional Edition (Windows hosted) Evaluation / Updates" \
HOSTID=ANY ISSUER="Freescale Semiconductor" ISSUED=20-jul-2020 \
NOTICE=NONE ck=119 SN="FSL - 31341727" TS_OK
# License for ANY
INCREMENT Win32_SA_Perf_EPPC_ADVANCED metrowks 10.5 19-aug-2020 \
uncounted 9338B4679A13 VENDOR_STRING="CodeWarrior for Power \
Architecture - Professional Edition (Windows hosted) \
Evaluation / Updates" HOSTID=ANY ISSUER="Freescale \
Semiconductor" ISSUED=20-jul-2020 NOTICE=NONE ck=126 SN="FSL - \
31341727" TS_OK
# License for ANY
INCREMENT Win32_Plugins_PPC_EmLinux metrowks 10.5 19-aug-2020 \
uncounted AF2689EB642A VENDOR_STRING="CodeWarrior for Power \
Architecture - Professional Edition (Windows hosted) \
Evaluation / Updates" HOSTID=ANY ISSUER="Freescale \
Semiconductor" ISSUED=20-jul-2020 NOTICE=NONE ck=177 SN="FSL - \
31341727" TS_OK
# License for ANY
INCREMENT WIN32_PLUGINS_GCC_Adapters metrowks 10.5 19-aug-2020 \
uncounted DD50CD09A9C3 VENDOR_STRING="CodeWarrior for Power \
Architecture - Professional Edition (Windows hosted) \
Evaluation / Updates" HOSTID=ANY ISSUER="Freescale \
Semiconductor" ISSUED=20-jul-2020 NOTICE=NONE ck=137 SN="FSL - \
31341727" TS_OK

 

0 Kudos
Reply

5,020 Views
wangrui_202077
Contributor I

HiYiping

License查看结果见附件,截取部分如下:好多插件是win32开头的?在win64 PC机上使用会受影响吗?同时我也在拔掉仿真器的情况下重新卸载干净后安装了codewarrior10.5.1软件,

功能Key

功能 WIN32_PLUGINS_DBG_PPC 10.5,状态: 15

功能 WIN32_PLUGINS_GCC_Adapters 10.5,状态: 15

功能 Win32_CFP_PPC 10.5,状态: 15

功能 Win32_PLUGINS_PPCCPU_COMM 10.5,状态: 15

功能 Win32_PLUGINS_PPCCPU_HOST 10.5,状态: 15

功能 Win32_PLUGINS_PPCCPU_PQ3 10.5,状态: 15

功能 Win32_Plugins_PPC_EmLinux 10.5,状态: 15

替代Key

(没有key)

另外想问,咱们新买的codewarrior tap仿真器需要load进去什么配置文件嘛?使用仍然报如下错误,请帮忙回答,非常感谢。

 

 

 

 

 

 

0 Kudos
Reply

5,020 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Rui Wang ,

Would you please refer to the following procedure to enable and capture CCS log to me to do more investigation?

Before connect to the target, please enable CCS log from "Run->Debug Configurations-><project>-core00_RAM_P2020_Download->Edit...->Advanced->Advanced CCS setting->Enable logging", and connect to the target from "Run->Debug Configurations-><project>-core00_RAM_P2020_Download->Debug", the CCS log will be printed in the console panel in CodeWarrior IDE.

 

Note: Please open the console panel from Window->Show View->Console, and if nothing displayed, please choose the correct session on the right top icon in the panel.If the CCS log in the console is truncated, please enlarge the console buffer from Window->Preferences->Run/Debug->Console->uncheck "Limit console output".

Thanks,

Yiping

0 Kudos
Reply