Hi all
I am trying to get CW v10 to download code to the P&E DemoJM board, which has the P&E multilink built-in.
(Win7, 64 bit machine)
The board works OK under CW 6.1. (XP system)
The 'P&E Connection Assistant' in the debugger shows that the board is connected 'USB-ML12: DEMOJM on USB1'
but it just says 'an error occurred, retry' when trying to download code.
and gives the error message 'HC GDI Protocol Adapter: Can't connect . The debugger cannot connect to the PE device.' when quitting the connection.
The first time I connected there was a (fast) code update of the multilink code in the board.
the HCS08 debugger is 10.0.0.FSL_b2619
Has anyone had CW working with this board? (or is there a bug as in CW v6.3+ which has the same problem)