Blog

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Blog

meghnaghole_1
NXP Employee
NXP Employee

This article is an overview of enabling 4K encoding capability on i.MX 8M Plus, along with varied experiments performed on i.MX 8M Plus to reduce the power consumption on SOC. 

Read more...

More
1 0 429
addiyi
NXP Employee
NXP Employee

DDR tool supports i.MX8M family, i.MX93 family and LX2160A\LX2162A. DDR tool is part of Config tools for i.MX offering configuration, inspection, optimization, vTSA, stressing and code generation. It can be downloaded from Config Tools for i.MX Applications Processors

DDR tool User Guide is part of  User Guide for Config tools for i.MX

Read more...

More
0 0 995
APraveen
NXP Employee
NXP Employee

The demo showcases ultra low power usage on a Sensor Hub and runtime power usage for SoC using Evaluation Kit (EVK) power measurement capability on i.MX8ULP.

Read more...

More
0 0 1,146
addiyi
NXP Employee
NXP Employee

DDR tool supports i.MX8M family, i.MX93 family and LX2160A\LX2162A. DDR tool is part of Config tools for i.MX offering configuration, inspection, optimization, vTSA, stressing and code generation. It can be downloaded from 

https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX

DDR tool User Guide is part of  User Guide for Config Tools for i.MX

 

 

Read more...

More
0 2 2,864
shaojun_wang
NXP Employee
NXP Employee

This document shows how to debug i.MX8MP uboot with TRACE32 debugger.
For Linux debug, please check https://community.nxp.com/t5/Blogs/Debug-i-MX8MP-Linux-with-TRACE32/ba-p/1582382

  1. Build uboot
  2. Run uboot and get relocate offset
  3. TRACE32 script
    3.1 Data.LOAD.Elf
    3.2 relocate offset
  4. Attach i.MX8MP board to TRACE32 debugger

 

 

Read more...

More
2 0 3,537
addiyi
NXP Employee
NXP Employee

DDR tool supports i.MX8M family and LX2160A\LX2162A. DDR tool is part of Config tools for i.MX offering configuration, inspection, optimization, vTSA, stressing and code generation. It can be downloaded from 

https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX

DDR tool User Guide is part of  User Guide for Config Tools for i.MX

 

 

Read more...

More
0 0 3,226
shaojun_wang
NXP Employee
NXP Employee

This article shows how to attach TRACE32 to i.MX8MP Linux and how to debug Linux with it.

Read more...

More
3 0 6,082
shaojun_wang
NXP Employee
NXP Employee

We already have application note AN13336 about running TFLM micro_speech example on Tensilica HiFi4 DSP on i.MX 8M Plus EVK.


In this document, TFLM micro_speech example will be upgraded to support i.MX DSP remote processors driver in newer Linux kernel, patch to support i.MX8QXP/i.MX8QM MEK will be provided, steps about how to download and install toolchain, how to build and run the example will be listed.

Hardware: i.MX8MP EVK, i.MX8QXP MEK, i.MX8QM MEK.
Software: Linux 5.15.52, TensorFlow Lite Micro

Read more...

More
2 0 3,545
xiaocong_fu
NXP Employee
NXP Employee

Step by step: load fusion fw to 8ulp flash


In this article, I'd like to share the steps to run fusion dsp fw in 8ulp, including all the issues I have encountered.

Pre-steps

To follow the steps, you will need:

Read more...

More
4 0 3,929
addiyi
NXP Employee
NXP Employee

DDR tool supports i.MX8M family and LX2160A\LX2162A. DDR tool is part of Config tools for i.MX offering configuration, inspection, optimization, vTSA, stressing and code generation. It can be downloaded from 

https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX

DDR tool User Guide is part of  User Guide for Config Tools for i.MX

addiyi_0-1658736521986.png

 

Read more...

More
0 0 3,157
petrstruzka
NXP Employee
NXP Employee

We are pleased to announce that Config Tools for i.MX Application Processors v11 are now available.

 

Read more...

More
0 0 2,173
addiyi
NXP Employee
NXP Employee

DDR tool supports i.MX8M family and LX2160A. DDR tool is part of Config tools for i.MX offering configuration, inspection, optimization, vTSA, stressing and code generation. It can be downloaded from 

https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX

Capture.PNG

 

 

 

Read more...

More
0 0 2,409
OliverB
NXP Employee
NXP Employee

After setting my new 16” M1Max Macbook Pro, I found some surprising results for the kernel compile time. The Ubuntu Virtual Machine on my M1 MBP compiled the i.MX Linux kernel faster than an Intel i9 3650 Dell Precision workstation running native Ubuntu. Since the comparison is a bit like apple to oranges, I tried to minimize the variables, and, I also compared an older i7 Dell Precision M4700 and a Xeon.

Read more...

More
1 4 4,351
CosminB05
NXP Employee
NXP Employee

An interactive tutorial on how to create your own MATLAB Simulink temperature sensor application by applying the model-based design approach, how to configure and use the i.MXRT1060 EVK using NXP MCUXpresso, a thermistor module and the IMXRT Toolbox.

Read more...

More
2 0 3,228
addiyi
NXP Employee
NXP Employee

User's Guide of DDR tool with support for i.MX8M family. DDR tool is part of Config tools for i.MX. It can be downloaded from 

https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX

Read more...

More
0 0 2,147
Kaixin_Ding
NXP Employee
NXP Employee

PyeIQ is written on top of eIQ™ ML Software Development Environment and provides a set of Python classes allowing the user to run Machine Learning applications in a simplified and efficiently way without spending time on cross-compilations, deployments or reading extensive guides.

Now PyeIQ 3.0.x release is announced. This release is based on i.MX Linux BSP 5.4.70_2.3.0 & 5.4.70_2.3.2(8QM, 8M Plus) and can also work on i.MX Linux BSP 5.10.9_1.0.0 & 5.10.35_2.0.0 & 5.10.52_2.1.0. And also, in latest PyeIQ 3.1.0 release, BSP 5.10.72_2.2.0 is also added into supported list.

This article is a simple guide for users. For further questions, please post a comment on eIQ Community or just below this article.

Read more...

More
5 1 6,265
BiyongSUN
NXP Employee
NXP Employee

This demo introduces the secondary boot of i.MX8QXP. 

This feature is very useful for such as OTA, rolling back. 

More
2 0 2,393
BiyongSUN
NXP Employee
NXP Employee

Some customer cases need hardware partition and the GPIO need to be allocated by bank.

It causes resource tensive. And some time, one GPIO bank assigned to the M4 side 32 bits of one bank are more than enough. And some customer cases need to use 1 or 2 bit to as board identification for the A core side. Because of the hardware partition, A core could not directly access the M4 partition resource.

Read more...

More
0 0 2,207
BiyongSUN
NXP Employee
NXP Employee

The example is to change the i.MX8QXP MEK debug uart(lpuart0) to the base board(lpuart2).

The lpuart2 is J37 on base board.

uart2-linux-uart2_L5.4.70_2.3.0.diff, uart2-u-boot-method1_L5.4.70_2.3.0.diff and uart2-u-boot-method2_L5.4.70_2.3.0.diff are the patches. 

Read more...

More
0 0 2,480
Eli_H
NXP Pro Support
NXP Pro Support

The NPU capability lies in the “sweet spot” for performance to enable real time response for common AI/ML problems. Combined with the video and vision co-processing capabilities, the i.MX 8M Plus will be the standard bearer for Edge ML/AI implementations

Read more...

More
3 0 3,377
BiyongSUN
NXP Employee
NXP Employee

Switch i.MX8MM debug port is not simple like i.MX6. Just change the bootargs.The changes include atf(Key changes), u-boot, Linux and systemd.

Read more...

More
2 0 6,731
addiyi
NXP Employee
NXP Employee

User's Guide of DDR tool with support for i.MX8M, i.MX8MM, i.MX8MN, i.MX8MP. DDR tool is part of Config tools for i.MX. It can be downloaded from 

https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX

Read more...

More
0 0 2,363
petrstruzka
NXP Employee
NXP Employee

We are pleased to announce that Config Tools for i.MX Application Processors v9 are now available.

Read more...

More
0 0 1,423
petrstruzka
NXP Employee
NXP Employee

We are pleased to announce that MCUXpresso Secure Provisioning Tool v2 is now available.

MCUXpresso Secure Provisioning Tool is a graphical user interface (GUI) tool covering the secure boot
process, aimed primarily at microcontroller customers. It provides unified GUI front-end over existing
command-line tools - FlashLoader, elftosb, blhost, cst.

Read more...

More
0 0 1,466
MeganHansen
NXP Employee
NXP Employee

Today, NXP announced an update to the eIQ™ Machine Learning Software Development Environment, becoming the first semiconductor vendor to implement the Glow neural network compiler for vision-, sensor- and voice-based ML applications. This new neural network compiler technology delivers unprecedented inferencing performance for NXP’s i.MX RT series of crossover MCUs.

Read more...

More
2 0 1,481
petrstruzka
NXP Employee
NXP Employee

We are pleased to announce that Config Tools for i.MX Application Processors v8 are now available.

The Config Tools for i.MX is a set of configuration tools that provide an efficient method
for evaluation and configuration of pins routing and DDR memory settings when designing
with NXP's application processors based on Arm® Cortex®-A cores, including i.MX MPUs.

Read more...

More
0 0 1,837
diego_dorta
NXP Employee
NXP Employee

PyeIQ is written on top of eIQ ML Software Development Environment and provides a set of Python classes allowing the user to run Machine Learning applications in a simplified and efficient way without spending time on cross-compilations, deployments, or reading extensive guides.

Read more...

More
11 0 10.1K
iWave
Contributor V

Have you recently been sceptical of using a contact-based access system in your office or a public place? This trait is a major concern in most places for a valid reason. An access surface in a public place is used by many individuals, which makes it a potential source for contracting the deadly Covid 19 virus. Taking this into account, iWave Systems, a leading embedded solutions provider, has successfully demonstrated an alternative solution using facial recognition technology. The solution helps customers with a zero-contact access application by using individuals' faces to authorize access to a commercial/industrial space, home/office, transportation, banking, and Government sites.

Read more...

More
0 0 1,553
iWave
Contributor V

iWave Systems and Crank Software partnered up to support rich graphics on the powerful NXP i.MX 8 series system on modules and SBC boards. Powered by NXP i.MX8 application processors, the SOM and SBC are optimized for sophisticated real-time computing in embedded applications, and Crank Software’s UI development software, Storyboard, complements the high-performing modules with an out-of-the-box GUI experience.

Read more...

More
0 0 1,553
iWave
Contributor V

The Debian based open-source Linux distribution Ubuntu finds its wide use across Desktop, Servers, Containers, and now in IoT and cloud applications. Being very secure and its OpenStack support, it is further getting adapted widely in high end embedded computing applications as well.

iWave systems rich i.MX8 System on Module and SBC product portfolio is supported with Yocto Linux, Android, and QNX BSP. Now iWave Systems is enabling the Bionic Beaver Ubuntu 18.04 LTS support to its latest i.MX8 Quad Max, Quad Plus, and i.MX8M, i.MX8M mini system on Modules and SBC products.

Wayland support in the BSP brings better performance, code maintainability, and security compare to X server. In Wayland, compositing is passive, which means the compositor receives pixel data directly from clients, and hence it reduces the latency compared to the X server. The GUI with the Wayland Compositor on the iWave i.MX8 board is shown below;

Read more...

More
1 0 1,987