sc_misc_board_ioctl to access the M4 partition from A core side

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

sc_misc_board_ioctl to access the M4 partition from A core side

BiyongSUN
NXP Employee
NXP Employee
0 0 1,684

Some customer cases need hardware partition and the GPIO need to be allocated by bank.

It causes resource tensive. And some time, one GPIO bank assigned to the M4 side 32 bits of one bank are more than enough. And some customer cases need to use 1 or 2 bit to as board identification for the A core side. Because of the hardware partition, A core could not directly access the M4 partition resource.

SCU has highest right to access any resource.

SC firmware for SCU has Remote Procedure Call (RPC) mechanism

Tags (1)