ILLEGAL_BP with MC9S08AW44

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ILLEGAL_BP with MC9S08AW44

1,794件の閲覧回数
Ciccio
Contributor I
Hi,
I use MC9S08AW44.
I have write little code for try PWM and input capture.
In attacment my code.

When I go to debug with Multilink I have a ILLEGAL_BP .
I have stepped with F10/F11 and in this istruction:
PTCDD |= (unsigned char)0x10;
the debugger exit to connection and alert me with:
"Can't communicate with the target processor! Please check your connections
between the cable and the target and make sure the taget has power."

The hardware connection are correctly: I have checked the wire with other software and work!

What's???
Thanks!
ラベル(1)
0 件の賞賛
返信
1 返信

1,140件の閲覧回数
mdelac01
Contributor I
I ran into a similar issue, using HCS08GT8.
The problem was the watchdog reset.  I was not resetting the dog.  By default the HC08 have the watchdog reset enabled.  Either disable it all toghther, or make sure you reset it regularly in your code.
 
Good luck
0 件の賞賛
返信