ADC on MC9S08 : 8bits; Hight speed; single conversion

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC on MC9S08 : 8bits; Hight speed; single conversion

1,344件の閲覧回数
Iko
Contributor II

Hi all i'll try to do this way. Could you confirm that this work?

 

First, i made an init:

 

 

static void adc_init(void)   {#ifndef FAKEDEV   APCTL1 = 0x0F ;  // Desable buffers I/O  for pins:   APCTL2 = 0x8F ;  // ADP 0->3;8->11;15;16->19; et 21->23   APCTL3 = 0xEF ;  // Pin PORT A;B and C   ADCSC2 = 0x00 ;  //raz & config reg SC2 . Start convertion by write on ADCSC1;   ADCCV  = 0x00 ;   //No save of compared value   ADCCFG = 0x00 ;  //Full power (hight speed)                    //Clock divide by 1                    //Standard sampling time (3.5 adc clocks)                    //8 bits operations                    //Bus clk selected   ADCSC1 = 0x1F ;  //Clear Flag conversion Complet (COCO)                    //NO Interrupt                    //Single conversion Mode                    //ADC DISABLE => ADCH = 11111;#endif   }

 

 

during my program, i call a simple function with channel parameter "voie"

 

 

static U8 adc_lecture(U8 voie)   {   U8 value = 0 ; //U8 is define as unsigned char#ifndef FAKEDEV   ADCSC1 = voie ;   while (! ADCSC1_COCO)      {      ;      }   value = ADCRL;   ADCSC1 = 0x1F ;#endif   return value ;   }

 

 

Do you think it's a good way?

ty in advance...

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

509件の閲覧回数
bigmac
Specialist III

Hello,

 

It is unclear to me why your functions might be "static".

 

While it will do no harm, the writing of the value 0x1F to ADCSC1 after each conversion is probably unnecessary since the ADC should automatically enter a lower power mode on completion of each conversion.

 

For your wait loop, the following code would suffice -

while (!ADCSC1_COCO);

 

 

Regards,

Mac

 

0 件の賞賛
返信

509件の閲覧回数
Iko
Contributor II

Hi big mac ^^

Ty for this answer.

 

I hadn't see that it go to low power after each conversion....

In addition, you write "should" (scuse i'm french ^^).

To be sure that it stop, i prefer write 0x1F to disable ADC...

 

TY ^^

0 件の賞賛
返信