Dear All,
We face to the g2d_blit issue while playing jpeg file.
[Issue]
Can't playing the specific jpeg content.
[Overview]
BSP: Linux L3.14.28_1.0.0
Gstreamer version: 1.2.3-r0
Board: Custom board
Serial Error log: g2d_blit_2d: fail with status -20
Gstreamer command:
$ gst-launch-1.0 filesrc location=sample.jpg ! jpegdec ! videoconvert ! imagefreeze ! imxg2dvideosink
[Questions]
Q1: Could you provide the fixed GPU library?
Q2: What is meaning of the error message "g2d_blit_2d: fail with status -20"?
[Related community thread]
https://community.nxp.com/thread/382961
https://community.nxp.com/thread/333569
Best Regards,
Keita
Solved! Go to Solution.
Hi Keita,
There is no offiicial gpu update for 3.14.28, I strongly suggest to move 3.14.52 with major GPU and g2d bug fixes, please check it:
fsl-arm-yocto-bsp.git - Freescale i.MX Yocto Project manifests
in case of error -20 it means gcvSTATUS_NOT_ALIGNED could be due to you are using a jpg image on imxg2dvideosink. please check it: https://community.nxp.com/thread/394565
Regards
Hi Keita,
There is no offiicial gpu update for 3.14.28, I strongly suggest to move 3.14.52 with major GPU and g2d bug fixes, please check it:
fsl-arm-yocto-bsp.git - Freescale i.MX Yocto Project manifests
in case of error -20 it means gcvSTATUS_NOT_ALIGNED could be due to you are using a jpg image on imxg2dvideosink. please check it: https://community.nxp.com/thread/394565
Regards
Dear All,
Do you have any update?
Best Regards,
Keita