Can i.MX6DQ ESAI network mode add padding bit?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can i.MX6DQ ESAI network mode add padding bit?

ソリューションへジャンプ
630件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6DQ ESAI.

I understand SSI network mode cannot add padding data in i.mx6 SSI in TDM mode .

Then, how about ESAI network mode?

ESAI network mode cannot add padding data as the following image also?

Screenshot+from+2015-01-12+18-44-27.png

Best Regards,

Satoshi Shimoda

ラベル(4)
タグ(1)
0 件の賞賛
1 解決策
474件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

ESAI is able to add padding data, as shown in above diagrams.

In ESAI network mode it can output/receive 32 bits per slot, set by

SLOT LENGTH=32, described in Table 25-6. ESAI Transmit Slot

Table 25-9. ESAI Receive Slot i.MX6DQ Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
1 返信
475件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

ESAI is able to add padding data, as shown in above diagrams.

In ESAI network mode it can output/receive 32 bits per slot, set by

SLOT LENGTH=32, described in Table 25-6. ESAI Transmit Slot

Table 25-9. ESAI Receive Slot i.MX6DQ Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛