Can i.MX6DQ ESAI network mode add padding bit?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can i.MX6DQ ESAI network mode add padding bit?

跳至解决方案
1,129 次查看
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6DQ ESAI.

I understand SSI network mode cannot add padding data in i.mx6 SSI in TDM mode .

Then, how about ESAI network mode?

ESAI network mode cannot add padding data as the following image also?

Screenshot+from+2015-01-12+18-44-27.png

Best Regards,

Satoshi Shimoda

标签 (4)
标记 (1)
0 项奖励
回复
1 解答
973 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

ESAI is able to add padding data, as shown in above diagrams.

In ESAI network mode it can output/receive 32 bits per slot, set by

SLOT LENGTH=32, described in Table 25-6. ESAI Transmit Slot

Table 25-9. ESAI Receive Slot i.MX6DQ Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
974 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

ESAI is able to add padding data, as shown in above diagrams.

In ESAI network mode it can output/receive 32 bits per slot, set by

SLOT LENGTH=32, described in Table 25-6. ESAI Transmit Slot

Table 25-9. ESAI Receive Slot i.MX6DQ Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复