Hello All,
when I tried to install LTIB for building (Imx-233 linux BSP) , It shows
Following package not installed in Ubuntu 12.04 and 14.04 ?
(LTIB is supported in Ubuntu 9.04 (we can't use it because it become absolute now) )
If following package are not in Ubuntu 12.04 and 14.04 , then what is the alternative package for it. Any help on this will be useful.
List of packages:
glibc-devel
zlib
zlib-devel
Regards,
Kishore P
Hi kishore poojari,
Which version ubuntu are you using? Is it 32bit or 64bit?
Best Regards
Dan
Hello Dan,
I am using 32 bit version.
Regards,
Kishore P
Hi Kishore,
We are also trying to install ltib on 32 bit ubuntu 12.04. We face the same issue. Could you please comment regarding the solution for this issue? Thanks.
Regards,
Ijaz Fazily
Hello Ijaz Fazily,
Please find the below link and refer read me file
http://www.mediafire.com/download/754x06o7gr6m466/VJ.tar.gz
For More info refer:
what I learnt: LTIB for UBUNTU 11.10 & error faced
Regards,
Kishore P
Thanks Kishore P.
Hi kishore poojari,
In the ltib/bin/Ltibutils.pm :
zlib | => sub { my @f = (glob('/usr/lib/libz.so*'), |
glob('/lib/libz.so*'), | |
glob('/lib64/libz.so*'), | |
glob('/usr/lib/i386-linux-gnu/libz.so*'), | |
glob('/usr/lib32/libz.so*'), | |
glob('/usr/lib/x86_64-linux-gnu/libz.so*') ); @f > 1 ? 1 : 0 }, | |
'zlib-devel' => sub { -f '/usr/include/zlib.h' }, |
Make sure lib.so point to the correct one in your system.
Besides, have you installed the packages needed by ltib?
Best Regards
Dan
Hello Dan,
I have installed all required package for ltib except
glibc-devel
zlib
snippet in In the ltib/bin/Ltibutils.pm:
zlib => sub { my @f = (glob('/usr/lib/libz.so*'),
glob('/lib/libz.so*'),
glob('/lib64/libz.so*') ); @f > 1 ? 1 : 0 },
'zlib-devel' => sub { -f '/usr/include/zlib.h' },
help me short out this issue..?
Regards,
Kishore P
Hi Kishore P,
Are you using 64bit ubuntu? If yes, you can follow the setting in ltib/bin/Ltibutils.pm I showed you and you can refer to the Compile L2.6.35_1.1.0_130130 for i.MX28 on Ubuntu 12.04 64bit OS and Compile L3.0.35_4.1.0 on Ubuntu 14.04 64bit OS to install the needed packages to the linux host PC.
Have a nice day
Best Regards
Dan