Hi all,
does anyone have an idea where to find example code for a software UART (just using Rx and Tx) via GPIO pins?
Issue is that MPC5744P has only two LinFlex modules and in the application a third one is required for baudrates up to 115kbaud.
Thanks
br
Guenter
Hi,
Here you can find an only example which is available for Panther UART at this time.
Hi Peter,
thanks. I found that one as well. However I'm looking for a piece of software where a UART can be emulated using 2 GPIO pins and timers and probably DMA to create a third UART for the device. The application requires three UARTs but on Panther only two are realized in hardware.
br
Guenter