Dear All,
We have a requirement where we need to run specific application on specific core of i.MX6Q. I want to know which hyper visor is available and tested on i.MX6Q?
Also if i.MX6Q supports Asymmetric Multi Processing mode? Do we have any port or document available explaining this?
Regards,
Dipen Patel
Hi Dipen
one can look at third-parties
http://community.arm.com/message/15766
https://community.freescale.com/docs/DOC-94513
AMP will be supported by freescale software on i.MX6SX (there is no support for other i.MX6x)
[PATCH 10/11] ARM: i.MX: Add i.MX6sx sabresdb support
Regarding running specific application on specific core one can look at SDK
Multicore Startup example and link below
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I have a similar requirement for a system i'm creating and it is safety critical. Is there any documentation on the i.MX6D, i.MX6Q or i.MX6SX and isolating the cores for asymmetric processing? I've seen the example but i'm looking for documentation from NXP that allows for AMP on these processors without using those specific OSes.