magic missmatch, response was 0x00000000 in imx7d-pico android things

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

magic missmatch, response was 0x00000000 in imx7d-pico android things

1,646 Views
neuberfran
Contributor IV

foto21.png

https://community.nxp.com/docs/DOC-105652 

Hi,


I have the link error below:
https://community.nxp.com/thread/518603

and I'm trying this:
https://github.com/boundarydevices/imx_usb_loader

I have this issue in that place, because not have file mx7d_usb_work.conf :

Please add support to imx7d-pico NXP SOM Module · Issue #109 · boundarydevices/imx_usb_loader · GitH... 

My question is:

How can I change this line: hid,1024,0x910000,0x80000000,1G,0x00910000,0x20000 in 

mx7_usb_work.conf to work correctly with imx7d-pico and resolve the topic issue?

editavel1.png

Labels (4)
0 Kudos
Reply
5 Replies

1,246 Views
igorpadykov
NXP Employee
NXP Employee

Hi NEUBER

such error may happen when for example uboot version does not match

to linux kernel, so may be recommended to rebuild all sources from scratch.

As imx7d-pico was developed by technexion, issue may be posted on its forum

https://www.technexion.com/solutions/iot-development-platform/android-things/ 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,246 Views
neuberfran
Contributor IV

igorpadykov  This company's forum does not accept posts. They do not answer my emails.Those people don't talk to me anymore. I was never rude. I have two complete kits practically unused. I can't even sell it.

@igorpadykov You have been following this case and maybe you can answer me something about mfgtool2. (I'm investigating, in detail, why this tool damage my device)

1) In photo121 (attached) What is the command blkdiscard for? Could leaving this command (8 minutes longer than it should: My other imx7d pico android things start kit died, again ) running on Host PC have damaged my device? What other photo list command (photo121) may have damaged my device?

Having left 8 minutes longer, may have made it jump from container </LIST> thus unduly going to the "eMMC-Brillo-uboot-fuse" Container ???

photo121.png - Google Drive 

2) Why my ucl2.xml don't have <!-- create partition --> Container ? (photo122)

photo122.png - Google Drive 

i.MX8MQ booting error? 

3) What about this (u said): 

You should modify software sources for "MCIMX7D5EVM10SD" part.

How can I do this? Will I have to remove the new chip and do this rewriting?

0 Kudos
Reply

1,246 Views
igorpadykov
NXP Employee
NXP Employee

Hi NEUBER

unfortunately this board uses mainline uboot/linux which are quite different than nxp software.

One can try to post issue on

How to get display and wifi working on PICO-PI-IMX7 - Linux on ARM - Engineering and Component Solut... 

Technexion PICO-PI-IMX7 - Yocto Project - Mender Hub 

Best regards
igor

0 Kudos
Reply

1,246 Views
neuberfran
Contributor IV

igorpadykov  and about my questions above about mfgtool2? I'm still investigating in detail what damaged my pico-imx7d SOM

e.g.:changed 8seconds to 8minutes in the messages above

Please help me

0 Kudos
Reply