We have a IMX7.D running android 7.1.2 with uboot as bootloader.
How to get a charging animation when device is switched off but user inserts charging pin ?
Currently device boots all the way up to the android which does not allow charging when device is turned off.
Please let me know if Im missing any information required to answer the question.
I will try it; seems promising. Thank you igor.
shivanipatel I checked the thread for battery animation in uboot. But it seems rather old.
we have
NXP N7.1.2_2.0.0 u-boot source
http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/snapshot/uboot-imx-n7.1.2_2.0.0-ga.tar.gz
Hi, Meet Thakkar
It would be helpful if you can provide below information:
In order to add boot animation in android, you can refer below links:
Hope, this will help you.
Regards,
Shivani
HI Shivani, Thank you for reply.
Yes. I am always able to charge the device even after its fully drained.
When device is "off" and user plugs in usb cable the PMIC boots up the CPU and uboot is loaded
after that android OS starts.
instead of starting android we just want to show charging status, so device does not boot Android OS and become fully functional.
I think this thread is more useful to me I will try to check that.->how to get the battery animation in u-boot