the i.MX6 issue of data that should not be received from SPI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

the i.MX6 issue of data that should not be received from SPI

988 次查看
massohy
Contributor II

Dear community member,

 

I have a issue on SPI in i.MX6 with yocto 3.14.52. I got a error transferring data via SPI as a master.

It is occurred in spi_imx_isr(). My software already complete to read all data, but rx_available() return true. So, spi_imx->txfifo will be minus, as a result, this function will return IRQ_HANDLED.

 

I added this code,

if(spi_imx->txfifo < 0) spi_imx->txfifo = 0;

but error was occurred again.

 

Please tell me why does rx_available() return true already data should be empty.

Or Is the patch existing to solve this problem?

 

Best regards,

标签 (1)
0 项奖励
回复
1 回复

893 次查看
igorpadykov
NXP Employee
NXP Employee

Hi mas

one can test with spi unit test (folder ../mxc_spi_test) and

compare ecspi registers with custom application case

[meta-fsl-arm,16/27] imx-test: Upgrade to 5.3 version - Patchwork 

L3.14.52 Demo Image

i.MX 6QuadPlus, i.MX 6Quad, i.MX 6DualPlus, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo Linux Binary Demo...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复