Example S32K144 LPIT DMA LPSPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example S32K144 LPIT DMA LPSPI

Example S32K144 LPIT DMA LPSPI

********************************************************************************************
* Detailed Description:
* LPIT_ch0 triggers DMA_ch0 periodically (1ms).
* Every trigger starts a minor DMA loop (8 bytes) transfer to the LPSPI1 TX FIFO.
* There are 8 minor loops per one major loop (64 bytes in 8ms).
* LPSPI1 sends two 32bit frames every 1ms.

* LPSPI1 RX data are masked, they are not stored in the RX FIFO.
* ------------------------------------------------------------------------------
* Test HW: S32K144EVB-Q100
* MCU: S32K144 0N57U
* Debugger: S32DS 2.2, OpenSDA
* Target: internal_FLASH
********************************************************************************************

Attachments
No ratings
Version history
Last update:
‎05-01-2020 08:22 AM
Updated by: