Processor Expert RAppID Suite for MPC5777M and S32 Design Studio Integration Multicore Example

File uploaded by stanish Employee on Dec 6, 2016Last modified by Diana Torres on Feb 24, 2017
Version 3Show Document
  • View in full screen mode

This application demonstrate integration Processor Expert (PE) RAppID Suite for  MPC5777M initialization tool with S32 Design Studio for Power v1.1.

There is a separate RAppID project and RAppID Workspace folder included in this project:




This multicore project first initializes the device (PinMux, Clocks, PIT timer). Each core toggles with one LED with different time period.

Z4_0 core: LED1...GPDO[0]

Z7_0 core: LED2...GPDO[1]

Z7_1 core: LED3...GPDO[2]



Yo can adjust the device initialization in PE RappID (open included workspace), generate the code and finally rebuild the project in S32DS.



  • Do not let generate PE_Types.h file since it includes some non-vle instructions mixed with VLE ones - this cannot be built by S32DS compiler.
  • linker command file generation needs to be disabled otherwise it generates HighTec specific keywords that S32DS GCC linker does not understand. 


Test HW:       MPC5777M-512DS, MPC57xx Motherboard

MCU:             PPC5777MQMVA8 0N78H

Debugger:    PeMicro USB-ML-PPCNEXUS

Target:           Debug (internal flash)

EVB connection:  USER LED1 connected to P8.0, LED2 connected to P8.1 LED3 connected to P8.2