Hi...
I am trying to unsecure flash permanently, without a 'mass erase',
and it isn't working: the device is unsecured, but reverts back to the
secured state after a reset.
Device is mc9s12c32
The data sheet states: "Once the MCU is unsecured, the Flash
security byte can be programmed to the unsecure state, if desired"
Pseudo-code for my latest version of code looks like:
WriteBAckDoorKey();
if( FlashIsUnsecured() )
{
EraseTopSector();
set NVFPROT to 'protected top 8K'
set NVFSEC to KEY_DISABLED, SEC_DISABLED
RestoreTopSector();
}
[We have been locking the flash, and unlocking it temporarily,
for quite a while now, and we are confident that the code 'blocks'
are OK]
I have tried a few variations on the above, (e.g. restoring the
trashed key in the 'if' block, setting NV_FSEC to KEY_ENABLED),
but have not had any success.
It seems as if permanently unsecuring the flash requires a mass
erase. This would make the operation similar to that of changing
the protection setting in NV_FPROT, and is logical enough.
Does anyone know if this is indeed the case?
With thanks, and best regards,
Sebastian
Solved! Go to Solution.
Hi...
Just to update:
We took your advice, and moved our 'key' to a different area, and
everything works as we intend it to.
Thanks for answering the question as well, i.e. confirming that
NVFSEC should be reprogrammable without mass erase. It
does, however, mean that I was trying to do it incorrectly...
I wonder if our use of NVFPROT at the same time was preventing
the reprogramming of NVFSEC, and causing the problem I was
seeing... I may revisit it one day out of curiousity.
Thanks once again,
Seb
Unsecure has nothing in common with the write protection. You can unsecure flash, but can't write-unprotect it. Resetting FPROT into not protected state requires operation in special single chip mode, which is only possible using BDM debugger.
If you need to be able to reprogram security bits, then you should not set NVPROT to protect sector containing security bits.
I don't really understand what for are you trying to disable security permanently. Once backdoor unsecure is complete, you can use Hiwave debugger in hot-plug mode. You can halt MCU, debug; if you wish read all the flash, mass erase and reflash chip with the same data but with security off.
Hi...
Ty for getting back to me...
I agree that what we are doing is quite unorthodox, and that we are
using the flash locking / unlocking feature very differently from what
it was intended for.
By way of (brief) background info:
We are using the state of FSEC as a means of controlling the re-
programming of the ECU... All programming commands
sourced on the CAN bus check this byte, and if the unit is secured,
they don't do anything. An 'authorised person' will lock the device
with a key known to himself only, and then the ECU can't be changed
without his unlocking it first. [quite literally: use of a BDM is impossible
once the unit has been assembled.]
electronically, it doesn't actually prevent us from programming it, nor
is it actually secure from hacking, but it does prevent impromptu code
changes.
Problem is: it is not always convenient to have to re-program the ECU
in the presence of the 'authorised person', and it would be much more
workable to be able to get him to unlock it, and then we give it back to him
2, 3 days later to re-lock.
Thing is, NVFSEC seems to be similar to NVFPROT, in that they may only
be re-programmed after a mass erase... And I was wondering if this was
actually the case, or if there is a trick that I'd missed.
Best regards,
Sebastian
PS: surprisingly enough, there was no problem 'protecting' the back door
key BAKEY with the FPROT mechanism. Buit I do agree that it is very risky,
in that the upper sector of code will be trashed (and the ECU written off!) if
something goes wrong...
Purpose of security bits is to prevent read out of firmware using BDM. Security bits don't control writeability of flash. To lock in application programming (programming over CAN in your case), you should use your own NV-variable in not write protected flash. Clearly this variable should not be placed in vectors area. Customizeable unlocking keys also should not be placed in vectors area.
But not when you replrogram NV security bits to disable security.
What authorised person is doing with your units? Is he debugging firmware in the field (setting breakpoints, doing some tests, inspecting variables etc), or just reflashing parts of your firmware? Disabling security is required only for debugging purposes. Write locking/unlocking for reprogramming over CAN or other non-BDM interface should not require disengage of security.
No, NVFSEC is not similar to NVFPROT. Reprogramming of NVFSEC doesn't require mass erase. Mass erase is required only to be able to reprogram your units using BDM.
No surprise here. Security bits and backdoor key is writeable until you set FPROT register (or NVPROT and then reset) to protect sector containing vectors, backdoor key, NVPROT and NVFSEC.
Yes, it's like shooting to your own foot.
Hi...
Just to update:
We took your advice, and moved our 'key' to a different area, and
everything works as we intend it to.
Thanks for answering the question as well, i.e. confirming that
NVFSEC should be reprogrammable without mass erase. It
does, however, mean that I was trying to do it incorrectly...
I wonder if our use of NVFPROT at the same time was preventing
the reprogramming of NVFSEC, and causing the problem I was
seeing... I may revisit it one day out of curiousity.
Thanks once again,
Seb
Yes, write protecting vectors sector makes whole vectors sector write protected, no exceptions are available for NVFPROT, NVFSEC and NVBACKKEY. Programming NVFPROT makes write protection permanent and removeable only using BDM debugger. Less permanent write/erase protection is available using FPROT register. Instead of programming NVFPROT you write protection setting to FPROT. Protection in this case is enabled until reset.