I'm using CW v10.0 and I'm trying to run a program on a ColdFire 52259. I used "Flash File to Target" and clicked "Program with Erase" and it appears to work correctly as it doesn't throw any errors in its output.
But when I go to Debug mode and it tries to run, I get the following error:
"'Launching task_example Int Flash Debug' has encountered a problem. Could not set PC to entry point. "
Does anyone have any idea what went wrong and how to fix this? It would be much appreciated.
I assume you are using OSBDM as connection?
I had that error message with an older OSBDM firmware.
You need to make sure that you are using the latest OSBDM firmware (on the board) and drivers (on the host) for MCU10.
You find the OSBDM firmware as well inside your MCU10 installation: {InstallDir}\Drivers\osbdm-JM60
BK