Using QN908x BLE SDK.
How can I find the handle_id for given attribute the simplest way on the connected BLE device?
Something like get_handle id for: service_hex/attribute_hex path
Or can I hard code handle ID, is it same for a BLE profile across iphone/android?
The longest and only way I found was:
gatt discover 0 -all // uses GattClient_DiscoverAllPrimaryServices
--> Discovered primary services: 3
--> Generic Attribute Start Handle: 1 End Handle: 5
- Service Changed Value Handle: 3
--> Generic Access Start Handle: 20 End Handle: 28
- Device Name Value Handle: 22
- Appearance Value Handle: 24
- Central Address Resolution Value Handle: 26
--> User Data Start Handle: 40 End Handle: 65535
- Serial Number String Value Handle: 42 <---- I'm looking for this number
gatt discover 0 -service service_hex
--> Discovered primary services: 1
--> User Data Start Handle: 40 End Handle: 65535 ---> misses 42
Can I use the absolute address of uuid to read out its value (with GattClient_ReadCharacteristicValue)?
What's the point of the uuid if not?
Hi,
I hope you are doing great.
The Attribute Protocol allows devices to identify attribute types using UUIDs regardless of the local handle used to identify them in a read or write request.
The client must use GattClient_DiscoverAllPrimaryServices to obtain the handles of the attributes it is interested in.
The handle id could be assigned in a different order.
A client may send Attribute protocol requests to a server, and the server shall respond to all requests that it receives.
Regards,
Mario