How can i make ready my imx8m Nano device for device creation in other word boot to qt? I examined yocto project documents, qt documents and imx8 documents but i didn't understand. Anyhow i don't even know if it's possible. I built yocto project for my imx8m Nano device however i have no idea about boot2qt part. Does anyone have experience in this regard?
Hello Muhammet Aydın,
The latest BSP Release (L5.4.3_1.0.0) supports the i.MX8M Nano and there is an image based in Qt5 available. This is the only supported Qt iteration on the BSP.
It is my understanding that Boot2QT was rebranded as Qt for Device Creation.
https://doc.qt.io/QtForDeviceCreation/
You would need to port it to your desired board. However, there are some third party boards from Boundary Devices that do support this stack:
https://doc.qt.io/QtForDeviceCreation/qtdc-supported-platforms.html
I hope this information helps!
Regards,