Hi,experts
our design info : i.MX8MQ with LPDDR4 3GB(Micron 6Gb-die * 4). and we want to change the LPDDR4 3GB(Micron 6Gb-die * 4) device to LPDDR4 2GB(Micron 8Gb-die *2) device.
when we use ddr stress tool to train our new board, we want to do LPDDR4 training to single channel ,
for example of action sequence is : do training to channel A --> do training to channel B.
please , help us confirm :
1: Can imx8m DDR stress tool do lpddr4 training only to single appointed channel in one time
2: if yes , how to set tool parameters or RPA file to achieve this goal ?
thanks.
hi, experts
could you please give us some hints about this question?
thanks
Yes, you can only use one channel (Channel A).
You can configure the bus width to 16 in RPA tool to enable only Channel A.
thanks Rita.
and how about single channel B ?
in fact , we encount a training failed issue. and we want to try to do training to single channel for the puopose of finding which channel failed. so we post this session on community.
OR , are there any registers we can read , which can show the failed status of which channel, which dbyte,and what is the failed training step ?
thanks.
You can configure the ddr in the https://community.nxp.com/docs/DOC-340179 script.
I will do further confirm for you, please wait.