Hello,
I have MIPI CSI-2 Camera (RAW10/12 Video Data 1080p30).
Is it possible to capture this video format on iMX.6 Quad?
Hello Vladimir,
Yes it is supported by the MIPI CSI2 driver.
Regards
Thank you for your answer!
I studied a lot of topics in the forum about this problem.
I have Toradex Apalis iMX6Q (Toradex Linux BSP based NXP Release imx_4.9.123_2.3.0_ga).
I make for my camera, which is based on the Sony IMX327 sensor, a driver based on ov5640.
I set in driver:
else if (ifparm.u.bt656.mode == V4L2_IF_TYPE_BT656_MODE_NOBT_12BIT)
{
csi_param.data_width = IPU_CSI_DATA_WIDTH_12;}
case V4L2_PIX_FMT_SBGGR12:
size = f->fmt.pix.width * f->fmt.pix.height * 2;
bytesperline = f->fmt.pix.width * 2;
break;
else if (cam->v2f.fmt.pix.pixelformat == V4L2_PIX_FMT_SBGGR12)
pixel_fmt = IPU_PIX_FMT_GENERIC_16;
And so far I have no results.
Buffer capture based on https://linuxtv.org/downloads/v4l-dvb-apis/uapi/v4l/capture.c.html
I also tried the changes described i.MX6Q capture raw(bayer) data and debayer
Nothing happened.