nxp@ve:~/Desktop/ltib-mpc8641hpcn-20080117$ ./ltib
defined(@array) is deprecated at /home/nxp/Desktop/ltib-mpc8641hpcn-20080117/bin/Ltibutils.pm line 395.
(Maybe you should just omit the defined()?)
ltib cannot be run because one or more of the host packages needed
to run it are either missing or out of date.
Please install/upgrade these packages and then re-try.
Package Minimum ver Installed info
------- ----------- ---------------
glibc-devel 0 not installed
zlib 0 not installed
rpm 0 not installed
rpm-build 0 not installed
ncurses-devel 0 not installed
m4 0 not installed
bison 0 not installed
Died at ./ltib line 1232.
Started: Thu Feb 6 12:13:18 2020
Ended: Thu Feb 6 12:13:19 2020
Elapsed: 1 seconds
Build Failed
Exiting on error or interrupt
Please Help me to solve this issue?
Thanks in Advance!
Please refer to https://community.nxp.com/thread/524166 .