nxp@ve:~/Desktop/ltib-mpc8641hpcn-20080117$ ./ltib
defined(@array) is deprecated at /home/nxp/Desktop/ltib-mpc8641hpcn-20080117/bin/Ltibutils.pm line 395.
(Maybe you should just omit the defined()?)
ltib cannot be run because one or more of the host packages needed
to run it are either missing or out of date.
Please install/upgrade these packages and then re-try.
Package Minimum ver Installed info
------- ----------- ---------------
glibc-devel 0 not installed
zlib 0 not installed
rpm 0 not installed
rpm-build 0 not installed
ncurses-devel 0 not installed
m4 0 not installed
bison 0 not installed
Died at ./ltib line 1232.
Started: Thu Feb 6 12:13:18 2020
Ended: Thu Feb 6 12:13:19 2020
Elapsed: 1 seconds
Build Failed
Exiting on error or interrupt
Hello river jeep,
You need to set up the network environment, install some required packages.
If you use Ubuntu OS, you could refer to the following script to install necessary packages.
#/bin/bash
# Install LTIB dependant packages
sudo apt-get install gettext libgtk2.0-dev rpm bison m4 libfreetype6-dev
sudo apt-get install libdbus-glib-1-dev liborbit2-dev intltool
sudo apt-get install ccache ncurses-dev zlib1g zlib1g-dev gcc g++ libtool
sudo apt-get install uuid-dev liblzo2-dev
sudo apt-get install tcl dpkg
# Packages required for 64-bit Ubuntu
# Do "uname -a" and see if the word "x86_64" shows up.
if uname -a|grep -sq 'x86_64'; then
sudo apt-get install ia32-libs libc6-dev-i386 lib32z1
fi
Thanks,
Yiping