i am complete beginner to microcontroller can you please tell me that which software do i use to upload boot loader to LPC1549JBD64 and which programmer should i use. Can stlink v2 will work or not please give me bootloader file for LPC1549JBD64 and LPC1549JBD48
Hi,
You can use LPC link-2. Firmware can easily be loaded into the board using the free LPCScrypt utility, which runs on Windows (7/8/10), MacOS and Linux. Note that when using LPCXpresso IDE or MCUXpresso IDE, no firmware programming is required.
I suggest using MCUXpresso IDE and LPCOpen drivers.
You can download MCUXpresso IDE and LPCOpen from the following links:
MCUXpresso IDE|Eclipse-based Integrated Development Environment (IDE) | NXP
LPCOpen Libraries and Examples | NXP
Regards
Soledad