I am attempting to use the ENET Adjustable Timer on the MIMXRT1064 EVK demo board.
I have been configuring the ATCR register to capture a time and the attempt to read it via ATVR. According to the reference manual the CAPTURE and RESET commands should both reset to 0 when the command completes. I have found that neither of the commands reset. Once I issue a RESET or CAPTURE command the corresponding bit stays high. When I read ATVR I always receive a 0.
Is there a condition where commands issued to the ATCR will not complete?
Thank you
Hello Brian,
MCUXpresso SDK for IMXRT1064-EVK software package provides [txrx_ptp1588_transfer] demo, which shows the way to use ENET driver to receive and transmit frame in the 1588 feature required cases.
Please find related demo with below default path:
\SDK_2.7.0_EVK-MIMXRT1064\boards\evkmimxrt1064\driver_examples\enet\txrx_ptp1588_transfer
Wish it helps.
Have a great day,
Mike
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------