CodeWarrior for Coldfire 7.1
Hi everyone,
I'd like to enable a breakpoint for when a variable reaches a given value.
The 'Condition' column in the Breakpoints view seems like it should do just that.
Unfortunately I couldn't find in the online manual how to write a condition.
I've tried to enter a string like "a == 2" but after hitting continue, not just the breakpoint was never hit but the IDE became irresponsive and I had to shut it down.
So, I suppose there should be another way of entering conditions.
Does anybode know whether that feature is supported in CodeWarrior for Coldfire? and how?
Thanks,
Emanuel
Hi,
i had exactly the same problem with a codewarrior 8.7 for powerpc. To solve it i had to download codewarrior 9.2 (always power architecture version).
greetings
Hello
Conditions should be specified using ANSI C syntax (i== 2) if you want to stop when global variable i is equal to 2.
If this is not working I would recommend you to submit a service request for that.
Click here to submit a service request.
Make sure to attach a reproducible project and installed product information to the service request.
To generate the required information:
- Start CodeWarrior
- Open the project
- Select "Help" -> "Pack and Go" and follow instructions on the screen.
Attach the generated .zip file to the SR.
CrasyCat