To set up static IP in MX8M?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

To set up static IP in MX8M?

2,811 次查看
wjdwogud137
Contributor I

Hi

I want to use MX8M as a static IP.

Use the connmanctl services in the description, but i don't have it.

/etc/network/interaces no files

I wonder how you can give me a static ip.

Thank you

标记 (2)
0 项奖励
回复
3 回复数

2,721 次查看
joanxie
NXP TechSupport
NXP TechSupport

you can try the command like "ifconfig eth0 xx.xx.xx.xx" when board boot up

0 项奖励
回复

2,721 次查看
molin_du
Contributor II

Hello Joan:

Is there any way that the board boot up with a fix IP ? not know how to config poky Linux (on Ubuntu it is easy ... )

0 项奖励
回复

2,719 次查看
joanxie
NXP TechSupport
NXP TechSupport

you can set "ip=static_ip_address" according to the Table 11. Common kernel boot parameters of enclosed file

0 项奖励
回复