Hi all,
I am trying to create a bootstrap image for iMX6 and the command mkimage fails like below:
$ mkimage -n imximage.cfg -T imximage -e 0x17000000 -d overlay_img bootstrap_img.bin
Error: imximage.cfg[1] - Invalid command(/*)
Further investigation shows that the error is caused by that there is c-type comments (/*...*/) in imximage.cfg file. When I remove all the c-type comments in the file, it works fine.
u-boot document does say that imximage.cfg accept comment line starting with '#' in the file. However, that file, which is coming together with u-boot source has c-type comments. I am thinking the file is involved in some u-boot compiling. How to convert that file to remove all the c-type comments automatically so it can be used in mkimage command?
Thanks,
Yan
Hi Yan
as this is specific uboot question, issue may be posted on uboot mail list:
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------