flashing the example code on to the RAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

flashing the example code on to the RAM

1,233 Views
nsnmaniram
Contributor III

hi,

is there a possibility to flash a example code on to the RAM using MCUxpresso IDE on IMXRT1050-EVKB board?

0 Kudos
Reply
2 Replies

1,083 Views
jeremyzhou
NXP Employee
NXP Employee

Hi maniram nagothi,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you to refers to the Building and Debugging Projects for RAM section in the attachment.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,083 Views
nsnmaniram
Contributor III

can you please provide the attachment?

0 Kudos
Reply