About pressure sensor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About pressure sensor

652 Views
r-kokubun
Contributor I

この状態で圧力センサーはありますか?

・絶対圧

・測定範囲6〜400kpa

・測定媒体蒸気/水

Labels (1)
Tags (2)
0 Kudos
1 Reply

568 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

I recommend the MPXHZ6400A, this pressure sensor is an…

  1. Integrated (on-chip calibrated, compensated and amplified)
  2. Absolute
  3. Analog output (from 0 to 4.75V)
  4. Measurement range from 20 to 400kPa (it is not possible to measure pressure below 20kPa)
  5. “Media Resistant” option, which is the default choice in sensor selection for an application that may call for added protection like vapor / water measurement.

 

MPXHZ6400A Datasheet: https://www.nxp.com/docs/en/data-sheet/MPXHZ6400A.pdf


Have a great day,
Jose

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos