MMA8451 motion and transient detection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MMA8451 motion and transient detection

1,238件の閲覧回数
tadeuszstudnik
Contributor I

Hi. 

It is posible to configure MMA8451 to detect motion and transient simultaneously?

I can configure MMA8451 to motion detection or transient but if i configure both and assing interrupt to int1 and int2, it doesn't work.

Thanks in anticipation!

ラベル(1)
0 件の賞賛
返信
1 返信

1,074件の閲覧回数
lisettelozano
NXP Employee
NXP Employee

Hello Tadeusz,

It is not possible to use the motion and the transient detection functions together.

However, the transient detection and the motion detection functions are similar except that in the transient detection the high-pass filtered data is compared. There is an option to disable the high-pass filter (0x1D: TRANSIENT_CFG register), in which case the behavior of the transient function will be the same as the motion detection allowing to have two motion detection functions. For this, please check section 6.5 of the datasheet and application note AN4071.

I hope this information can be helpful.


Have a great day,

Paulina

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信