Hello, Dear Commity,
I am trying to config CSI0 register for imx6 dual (MCIMX6D5EYM10AD).
I need use CSI0 to capture YUV422(YUYV) sensor data. Detail is listed below:
1.pin : CSI0_DAT[12-19] 8bit
2.timing protocol: Gated mode
3.YUV color: YUV422 16bit/color
And then,with <i.MX 6Dual6Quad Applications Processor Reference Manual>,I config IPU0_CSI0_SENS_CONF register like this: 0x0400C900, but it received data from CSI0_DAT[4-19]. For example,send aa 55,but the data it received is 00 aa and 00 55.
So the question is how I config the CSI0 to make it work on CSI0_DAT[12-19] and receive 16bit/color data.
Thanks!
Thanks very much for your reply!
But I want to get yuv 16bit in two cycle with port IPUx_CSI_12 to IPUx_CSI_19.
Can it be available?
yes, it's correct
Got it. Thanks for your reply.
since you want to get yuv 16bits one cycle, pls connect IPUx_CSI_4 to IPUx_CSI_19
for more detailed information, pls refer to the Table 62. Camera Input Signal Cross Reference, Format, and Bits Per Cycle of data sheet
Thanks very much for your reply!
But I want to get yuv 16bit in two cycle with port IPUx_CSI_12 to IPUx_CSI_19.
Can it be available?