I have some problems in S32K 146
when I used FTM mode,I used FTM3 mode ,but all the FTM clock source are opend ,then I turn off the extra for FTM and use PE to generate code and save it .
The second time I opened the project ,all the FTM clock has been opened again, I don't know why .
I hope that kind people can help me
Solved! Go to Solution.
Hello,
I was able to reproduce the behavior you mentioned. This is a known issue, it has been already fixed, but with the SDK v3.0.1 release.
Best regards,
Victor.
Hello,
I wasn't able to reproduce the behavior you mentioned.
What version of the S32DS are you using?
What version of the SDK are you using?
Is this an issue of a single project or all your projects behave like this?
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
HI.
thanks for you answer.
The version of the SDK is 2.0.0
The version of the S32 DS is S32 Design Studio for Arm® 2018.R1
This is an issue of a single project just in S32 DS
I try to use the SDK for 3.0.0 ,and had met the same question.
Hello,
I was able to reproduce the behavior you mentioned. This is a known issue, it has been already fixed, but with the SDK v3.0.1 release.
Best regards,
Victor.