WiFi / wlan on core-image-full-cmdline-imx8mqevk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

WiFi / wlan on core-image-full-cmdline-imx8mqevk

1,715 Views
purnank
Contributor I

I am trying to get WiFi up and running on iMX8, but unfortunately i am not able to get Interface wlan0 listed on the board.

Through various threads,  I have tried to wpa-supplicant,iw, etc. wireless pacakges but all steps have gone to vein. 

Any suggestion which steps I am missing to get WiFi enabled on core-image-full-cmdline-imx8mqevk ?

Here is my conf/local.conf

MACHINE ??= 'imx8mqevk'
DISTRO ?= 'fsl-imx-xwayland'
PACKAGE_CLASSES ?= "package_rpm"
EXTRA_IMAGE_FEATURES ?= "debug-tweaks"
USER_CLASSES ?= "buildstats image-mklibs image-prelink"
PATCHRESOLVE = "noop"

BB_DISKMON_DIRS ??= "\
 STOPTASKS,${TMPDIR},1G,100K \
 STOPTASKS,${DL_DIR},1G,100K \
 STOPTASKS,${SSTATE_DIR},1G,100K \
 STOPTASKS,/tmp,100M,100K \
 ABORT,${TMPDIR},100M,1K \
 ABORT,${DL_DIR},100M,1K \
 ABORT,${SSTATE_DIR},100M,1K \
 ABORT,/tmp,10M,1K"
PACKAGECONFIG_append_pn-qemu-native = " sdl"
PACKAGECONFIG_append_pn-nativesdk-qemu = " sdl"
CONF_VERSION = "1"

# UBOOT_CONFIG = "emmc"

DL_DIR ?= "${BSPDIR}/downloads/"
ACCEPT_FSL_EULA = "1"

# gmmmkkk
IMAGE_ROOTFS_EXTRA_SPACE = "4000000"

IMAGE_INSTALL_append += " cmake curl git subversion python-pip python-click python-cryptography python-pycparser python-cffi"

IMAGE_INSTALL_append += " connman connman-client"
IMAGE_INSTALL_append += " wpa-supplicant iw"

CORE_IMAGE_EXTRA_INSTALL += " packagegroup-base-wifi"

IMAGE_INSTALL_append += " linux-firmware-ath9k"

IMAGE_INSTALL_append = " \
kernel-modules \
kernel-module-qualcomm \
udev-extraconf \
wireless-tools \
wpa-supplicant \
"

INHERIT+="toaster buildhistory"

Tags (1)
0 Kudos
Reply
3 Replies

1,196 Views
MichaelBMiner
Contributor IV

Has a solution to this been found?

0 Kudos
Reply

1,221 Views
josephzhou1
Contributor V

ok

Best Regards,
Joseph Zhou Jianhui / Senior Embedded Software Engineer, Singapore
0 Kudos
Reply

1,452 Views
igorpadykov
NXP Employee
NXP Employee

Hi Purnak

one can try guidelines provided in sect.4.13.7 Configuring WLAN from User Space

attached Linux Manual with Demo Umages from

i.MX Software | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply